PIAB’s new P6040 provides a modular solution in a smart design

PIAB introduces its P6040 pump range. Featuring patented COAX® technology, the P6040 can reduce energy costs by up to 25% or more compared to other methods of generating vacuum. With flexible mounting options, an extensive performance range and optional control functions, the P6040 is highly adaptable and well suited for most industrial vacuum applications.


Latest news


Learn how you can benefit from the revolutionizing COAX® technology:

www.coaxtechnology.com


Customer testimonials

UK printing company grows business and reduces energy and service costs

Occupying less space than the previous system, Arkle Print was able to reorganize machinery to increase efficiency. The company plans to continue replacing older mechanical pumps with PIAB technology to capitalize on the space, service and energy savings.  Read more »

Solutions for the consumer goods industry

PIAB will be exhibiting at the Pack Expo International trade show in Chicago from November 9-12. Products shown in the booth will be vacuum pumps, suction cups and vacuum conveyors that are suited for the consumer goods industry.

Read more »

 


Product news

7/4/2008

Greatly reduces air consumption

AVM™2 (Automatic Vacuum Management) is a further development of the well-known AVM™, which can re... Read more »
7/4/2008

Control functions in one compact unit

The control unit (CU) has integrated, electrically controlled on/off and blow-off valves. The CU ... Read more »
6/23/2008

For handling of lightweight products

PIAB introduces one more suction cup to the BL40-4 family of specially designed bag-handling suct... Read more »

Trade shows

Pack Expo International Chicago, November 9-12, 2008

Click here for information on FREE registration.

More trade shows »